Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to register an ION service

Issue
An ION Service is removed after installation or does not get installed

Environment
Command Prompt running as administrator

Product
ION Enterprise 6.0
StruxureWare Power Monitoring (SPM) 7.0
Power Monitoring Expert 7.2
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021​​​​​​​
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Power Monitoring Expert 2024

Cause
Many different reasons could cause an ION service to not exist. If the issue is during the installation process it is recommended to contact technical support for assistance.

Resolution 1:
Any of the ION services can be registered from the command line by running:
"-Service"
and unregistered with:
"-UnregServer"

The EXE files are located in \system\bin folder.
Below is an example of registering the OPC service.

Command Prompt Example to Register a Service

Below is a list of the executables associated with each ION service. Not all services are available in each version of the software:

ServiceExecutable
ION Alert MonitorAlertMonitor.exe
ION Cloud AgentCloud.Agent.Pme.Service.exe
ION Component IdentifierPMLexeMonikers.exe
ION Connection ManagementPMLConnectionManager.exe
ION Diagnostics and UsageIONDiagnosticsAndUsage.exe
ION Event WatcherIONEventWatcherService.exe
ION Log Inserterlogsrv.exe
ION Log Subsystem RouterLogSubsystem.Service.exe
ION Managed CircuitLogicalDevice.AutoConfig.ServiceHost.exe
ION Network RouterPMLNetman.exe
ION OPC Data AccessION.OpcDaServer.exe
ION Power Quality AggregationIONPowerQualityAggregator.exe
ION PQDIF ExporterPQDIFExporter.exe
ION QueryQueryServer.exe
ION Real Time DataIONServices.exe
ION Report SubscriptionIONReportSubscriptionService.exe
ION Sitesiteserv.exe
ION Software Alarm or
ION Software Data Processing
DataProcessorService.exe
ION Software Modbus GatewayModbusGatewayService.exe
ION Virtual Processor vip.exe
ION XML Subscription WebReach.XMLSubscriptionService.exe
ION XML Subscription StoreSubscriptionStore.exe

Resolution 2:

If the first process does not work and/or throws an error, then a different command can be used. Windows has a built-in command named "sc.exe delete". The format for using this is command is: sc.exe delete <ServiceShortName>

To find the short name of each service Power Monitoring Expert uses go to Registry Editor (you can go to Windows > Run > regedit.exe) and to the path Computer\HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Schneider Electric\Power Monitoring Expert\[Product Number associated with version].

You can then press the carrot/arrow beside the product number to expand the options below and the carrot/arrow beside ServiceMetadata to expand the folders within that one. This will provide the short name for all the Power Monitoring Expert services. See the screenshot below:

ServiceMetadata showing the PME services in Registry Editor

To recover these services that have been deleted, a reconfigure of the Power Monitoring Expert software can be done from the installer Window.