Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the control be flashed to a newer version on ATV312 and ATV212 drives?
Issue:
Reflashing the firmware inside the main control board on the ATV312 and ATV212 drives

Product Line:
Altivar ATV312 and ATV212

Environment:
All

Cause:
Needs to reflash the firmware on the ATV312 and ATV212 drives.

Resolution:
Firmware version of the ATV212 and the ATV312 drive cannot be flashed.