How can we help you today?

Does an EGX100 or EGX300 have a fiber optic connection port?

Issue:
A user would like to connect to an EGX gateway via a fiber optic connection.

Product Line:
EGX100
EGX300

Cause:
A user requires a fiber optic connection to the EGX gateway.

Resolution:
The EGX100 and EGX300 gateways do not have an on board fiber optic port therefore a direct fiber optic connection to the gateway is not possible.

Alternate Option:
A user can purchase and EGX in a Factory Assembled enclosure that contains a (4-Copper & 1-Fiber) Ethernet switch. The enclosure can be purchased for indoor or outdoor use.

Please reference page 33 of the attached factory assembled enclosure selection guide for part numbers.

Schneider Electric Nigeria

Attachment(s)
Factory Assembled Enclosures 2013.pdf [2.45 MB]