Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What will cause the E-FLEX drive to fault on HMI comm's fault after running in hand mode for a certain period to time?


Issue:
E-FLEX drive causes to fault on HMI comm's fault after running in hand mode for a certain period to time.

Product Line:
E-FLEX ATV61 Enclosed VFD


Resolution :
In an E-FLEX in hand mode the ATV61 uses the HMI for the speed reference signal.   If the Display standby mode is enabled, the keypad will shut down after the a specified period of time.  When the keypad shuts down, the drive looses the frequency reference that is set by the HMI causing an HMI fault on the VFD.   When the ATV61 is used in an E-FLEX, the standby function should not be enabled.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)