Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In Control Expert, how do I add the Ethernet and Remote IO Drops to a Quantum CPU application?
Issue:
In Unity Pro, how do I add the 140CRA31200 to a rack?

Product Line:
Unity Pro, 140CRA31200

Resolution:
To enable Ethernet RIO you must add a 140CRP31200 to the local rack.  There will be another node below the Local Quantum Drop called EIO bus.    Open the EIO bus, <double-click> on the drop (square box) and select your slot size.  Once that is complete, you will see the Quantum slot rack with a 140CRA31200.

To enable S908 RIO you must add a 140CRP93x00 to the local rack.  There will be another node below the Local Quantum Drop called RIO bus.    Open the RIO bus, <double-click> on the drop (square box) and select your slot size.  Once that is complete, you will see the Quantum slot rack with a 140CRA93100.