Issue:
Availability of DC bus plate for size 10 ATV61/71 drive.
Product Line:
ATV61, Altivar 61, ATV71, Altivar 71
Environment:
Frame size 10. ATV61HD90M3X, ATV61HC13N4, ATV71HD75M3X, ATV71HC11N4
Cause:
None
Resolution:
Due to safety reasons, Schneider Electric does not offer the DC bus plates separately for the ATV61 or ATV71 drives. Contact Schneider Electric Industrial Repair Services to have the drive sent in for repairs. ph 800-950-9550
Availability of DC bus plate for size 10 ATV61/71 drive.
Product Line:
ATV61, Altivar 61, ATV71, Altivar 71
Environment:
Frame size 10. ATV61HD90M3X, ATV61HC13N4, ATV71HD75M3X, ATV71HC11N4
Cause:
None
Resolution:
Due to safety reasons, Schneider Electric does not offer the DC bus plates separately for the ATV61 or ATV71 drives. Contact Schneider Electric Industrial Repair Services to have the drive sent in for repairs. ph 800-950-9550
Released for:Schneider Electric Nigeria