Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PME Adding additional digits of precision to web reports

Issue
System Manger Software(SMS) has 3 digits of resolution in their web reports. After migrate to PME, most of the reports provide two digits of resolution.

Product Line

Power Monitoring Expert 7.2

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024



Environment
Web Reporter in PME

Cause
The reports in PME are designed to have two digits of resolution.

Resolution

  1. Navigate to the folder where PME/SPM is installed(as shown in the below example):

C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\web\ReportDepot\ION Reports\ION Report Packs\Default Reports

  1. You will see RDL files for each report in that report pack. Open up the .RDL file in Notepad.
  2. Replace <Format>N2</Format> with <Format>N3</Format>
  3. Save the file.