Issue
A user would like to install additional meters into a HDM meter cabinet.
Product Line
PowerLogic® High Density Metering
Environment
HDM Enclosures Meter Installation
Cause
An auxiliary harness is needed to install additional meters in a HDM enclosure.
Resolution
The Auxiliary Harness Assembly Kit is used when adding a new row of meters to the metering cabinet in the PowerLogic® High Density Metering System.
The auxiliary harness accommodates up to four meters and is used in rows 2, 3, or 4 depending on the number of meters installed and the model of the cabinet.
The Auxiliary Harness Assembly Kit Instruction Bulletin is attached to this article.
A user would like to install additional meters into a HDM meter cabinet.
Product Line
PowerLogic® High Density Metering
Environment
HDM Enclosures Meter Installation
Cause
An auxiliary harness is needed to install additional meters in a HDM enclosure.
Resolution
The Auxiliary Harness Assembly Kit is used when adding a new row of meters to the metering cabinet in the PowerLogic® High Density Metering System.
The auxiliary harness accommodates up to four meters and is used in rows 2, 3, or 4 depending on the number of meters installed and the model of the cabinet.
The Auxiliary Harness Assembly Kit Instruction Bulletin is attached to this article.
Released for: Schneider Electric Nigeria