Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the thermal derating of Domae MCBs?
Are there any difference between the reference/standard temperature for Acti 9 and Domae MCBs?

Unlike Acti 9 MCBs (tested at 50°C), Domae MCBs are tested at 30°C. The derating tables for this range can be found attached.

Schneider Electric Nigeria

Attachment(s)
Domae Derating and characteristics.xls [27 KB]