Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find more information on enclosed 575V C-Flex drives?
Issue:
Customer wants an enclosed ATV61 or ATV71 drive for 575V.

Product line:
C-Flex, 8838CFD

Environment:
All

Cause:
No selection for ATV61 drives at 575V.

Resolution:
See the attached brochure for C-Flex product.  This product is only sold in Canada and do not have UL approvals.


Schneider Electric Nigeria

Attachment(s)
CFLEX_CA-EN.pdf [257.44 KB]