Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an CRF fault on the ATV31 and ATV312 drives?
Issue:
CRF fault on the ATV31/ATV312 drives.

Product Line:
Altivar ATV31 and ATV312

Environment:
All

Cause:
Powered down the drive and when they powered it back up it tripped on CRF and will not clear.

Resolution:
CRF is an internal precharge fault.  Power cycle.  If the fault does not clear you will need to replace the drive.

Schneider Electric Nigeria

Attachment(s)
Program BBV46385_03 ATV312.pdf [2.6 MB]