Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you set up the ATV61 or ATV71 drive to fallback to set speed when it drops its network connection?
Issue:
Set up the drive to fallback to set speed when it drops its network connection

Product Line:
Altivar ATV61 ATV71 using serial communications

Environment:
All

Cause:
Wants to the ATV61 drive to fallback to a fixed speed when the drive drops its network connection.

Resolution:
You can program the drive to do a fallback speed under network fault manager in menu 1.8 FLT management.
Programming
Set your Access level to Advanced in the Main Menu.
Menu 1.8 FLT menu
Com fault manager enter
Network fault manager set to LFF or Fallback speed.