Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why M218 can not keep the retain data after power off?
If you define a variable like "aaa", and you move it to %MW0. %MW0 is in retain area, but variable "aaa" is not a retain data, so "aaa" will over-write the %MW0 value, which cause %MW0 can not retain data. If you want variable "aaa" to keep data, you just define the variable as retain variable.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: