Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ATV12 drives be programmed to do an auto/manual between a 0 to 5vdc and a 4 to 20mA analog signal?
Issue:
Wants to program the ATV12 drives to do an auto/manual between a 0 to 5vdc and a 4 to 20mA analog signal.

Product Line:
Altivar Machines, Altivar 12

Environment:
All models and serial numbers

Cause:
Needs to have a logic input that can switch between hand and auto or 0 to 5vdc and 4 to 20mA signals.

Resolution:
No, the ATV12 does not have the ability to switch between two analog inputs.  There is a force to local input that can be assigned to switch over from the Ref 1 analog signal to a remote keypad display or local display on the face of the drive.