Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Error 1500 "Another Installation is in Progress you must complete the installation before continuing this one" when trying to install Vijeo Designer?
Issue
Error 1500 "Another Installation is in Progress you must complete the installation before continuing this one" when trying to install Vijeo Designer?

Product Line
Vijeo Designer

Environment
Vijeo Designer Buildtime Installation in Windows

Resolution
This is an InstallShield error message.  Most commonly, it means that another instance of InstallShield is running.  Go to the Windows Task Manager and end all processes for Msiexec.exe or Msiexec.exe *32.  Then run the install for Vijeo Designer again.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings