Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to recover from corrupted firmware or unresponsive APC Digital IP KVM - models KVM1116P, KVM2116P, and KVM2132P


Issue

The APC Digital IP KVM firmware upgrade has failed or gone awry and the KVM is not functioning properly.

The APC Digital IP KVM is found to be unresponsive or will not boot properly (such as with a blank screen with or without a mouse pointer).


Products

  • Rack Accessories - KVM Switches
    • KVM1116P
    • KVM2116P
    • KVM2132P


Environment

  • All serial numbers
  • All firmware versions


Cause

This process should be used to try and recover an unresponsive KVM switch, such as after a failed firmware upgrade or corrupted firmware that causes the KVM not to boot.

Resolution

On the front panel, hold the pinhole Reset button and simultaneously power on the unit. See below for reference.


KVM


This will revert the KVM back to factory default firmware version and settings. The unit can then be upgraded to the newest firmware available, found on apc.com/support, through the local console or web interface.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings