What is the "Life" (MTTF) of ATV61/71?
Issue:
"Life" (MTTF) of ATV61/71
Product Line:
All ATV61 and ATV71
Environment:
All models and serial numbers.
Cause:
None
Resolution:
The MTTF (Mean Time To Failure) varies based on the Drive's part number. Please refer to the attached Excel sheet.
Released for: Schneider Electric Nigeria