Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What do you do with the DC choke on an ATV61 or ATV71 high horse power drive when mounting a flange kit?
Issue:
Mounting an ATV61 with DC choke and a flange kit.

Product Line:
ATV61 ATV71 HHP Drives

Environment:
All serial numbers for ATV61 and ATV71 Drives

Cause:
N/A

Resolution:
When using the flush mount kit, the manual for the drive advises removing the dc chokes from their chassis and mounting them directly to the back pan of the enclosure.
See attachment.

Schneider Electric Nigeria

Attachment(s)
Flange Mounting with heatsink outside the enclosure.png [320.15 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings