Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why am I getting "Error 1800 [Target] can not find define target machine" when downloading to the HMISTU655/855?
Issue:
Why am I getting "Error 1800 [Target] can not find defined target machine" when downloading to the HMISTU655/855?

Product Line:
HMISTU655, HMISTU855, HMIS5T
Vijeo Designer

Environment:
HMI Configuration Software download to physical HMI

Resolution:
HMISTU family HMIs manufactured before 2012/03/12 were labeled on the back sticker specifically "HMISTU655" and "HMISTU855" these were the 3.5" and 5.7" screen sizes respectively.
The HMISTU655 and HMISTU855 did not have interchangeable front LCD screens and thus were manufactured with separate labels.

After this date, the HMISTU family supports swappable 3.5" and 5.7" screens, and the rear module is labeled "HMIS5T".
Nowadays,
- if you order an HMISTU655, it will come with a combination of the HMIS5T rear module + HMIS65 (3.5" screen)
- if you order an HMISTU855, it will come with a combination of the HMIS5T rear module + HMIS85 (3.5" screen)

So the download Error 1800 for the HMISTU family is often attributed to this difference.
Please confirm the label on the back of the rear module of the HMI matches the model number that is selected in Vijeo Designer.
e.g.
If the sticker reads "HMIS5T", please select the HMIS5T in the Target Type of the Vijeo Designer project.
If the sticker reads "HMISTU655", select the HMISTU655 in the Target Type of the Vijeo Designer project.
If the sticker reads "HMISTU855", select the HMISTU855 in the Target Type of the Vijeo Designer project.