Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PowerSCADA Expert (PSE) ION Protocol Help File
Issue:
Setting up/Troubleshooting an ION protocol device in PowerSCADA Expert (PSE).

Product Line:
PowerSCADA Expert 7.30
PowerSCADA Expert 7.40
PowerSCADA Expert 8.0

Environment:
PSE projects with ION protocol devices.

Cause:
Since the ION protocol is newly supported by PSE, it is useful to have a help document that describes how the ION devices communicate and how their tags are addressed.

Resolution:
Attached is the help file for the ION Driver. Some of the key topics that this help file covers are: Configuring Variable Tags, Supported Data Types, .ini Parameters, and Ethergate connections.

Schneider Electric Nigeria

Attachment(s)
ION.zip [1.55 MB]