Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
DLF3000 fails with error "Syntax error or access violation"

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

Issue
When adding a device routing in DLF3000, the following error appears.
DLF3000 fails with error "Syntax error or access violation" Language

Product Line
DLF3000

Environment
Upgrading firmware on PowerLogic devices

Cause
DLF3000 does not have enough privileges to add device routing.

Resolution
Run the application as an administrator by right clicking on the DLF3000 icon and selecting "Run as administrator". Once the application is open, proceed to adding device routing as before.

DLF3000 fails with error "Syntax error or access violation" Language

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: