Issue:
"The Main Drive or Secondary Drive is full. Runtime cannot execute" appears on the Magelis when trying to install an application.
Product Line:
XBTGC/GH/GK/GT, HMIGTO/STO/STU
Resolution:
This error message can appear when the Magelis does not have a CF card/SD card installed. To confirm, goto the Data Locations in Vijeo Designer and check if you have "User Application", "Data Files / Forms", "Recipes", or "Web Server" set for Secondary Drive. If yes, then this means that you need to have a CF/SD card (depending on unit) installed in the unit. Once you add a CF/SD card, reloading from the USB stick complete successfully. Alternatively, you may set the data locations to use Main drive if you do not have a secondary or optional drive.
"The Main Drive or Secondary Drive is full. Runtime cannot execute" appears on the Magelis when trying to install an application.
Product Line:
XBTGC/GH/GK/GT, HMIGTO/STO/STU
Resolution:
This error message can appear when the Magelis does not have a CF card/SD card installed. To confirm, goto the Data Locations in Vijeo Designer and check if you have "User Application", "Data Files / Forms", "Recipes", or "Web Server" set for Secondary Drive. If yes, then this means that you need to have a CF/SD card (depending on unit) installed in the unit. Once you add a CF/SD card, reloading from the USB stick complete successfully. Alternatively, you may set the data locations to use Main drive if you do not have a secondary or optional drive.
Released for: Schneider Electric Nigeria