Issue:
Does the ATS22 soft starters come with built in overload protection?
Product Line:
Altistart ATS22
Environment:
All
Cause:
Needs to know if the ATS22 soft starter has a built in overload protection
Resolution:
Yes, the ATS22 soft starters have built in overload protection.
The default motor thermal protection is IEC class 10.
You can adjust this value in the programming in the SEt menu.
Parameter tHP
Does the ATS22 soft starters come with built in overload protection?
Product Line:
Altistart ATS22
Environment:
All
Cause:
Needs to know if the ATS22 soft starter has a built in overload protection
Resolution:
Yes, the ATS22 soft starters have built in overload protection.
The default motor thermal protection is IEC class 10.
You can adjust this value in the programming in the SEt menu.
Parameter tHP
Released for: Schneider Electric Nigeria