Issue:
Looking for the SCCR ratings for ATV61 or ATV71, 18 pulse drives ?
Product Line:
ATV61 / ATV71
Environment:
PowerGard 18 Pulse Drives
Cause:
None
Resolution:
PowerGard enclosed drive controllers have a short-circuti current rating of 100 kA @ 480 V (RMS symmetrical).
See Altivar® 61/71 PowerGard™ Class 8839 Type CPD 18-Pulse Adjustable Speed Drive Controllers Instruction Bulletin 30072-451-53 for details.
https://www.se.com/us/en/download/document/30072-451-53/
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for: Schneider Electric Nigeria