Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ATV12 drive have a type 1 conduit kit option?

Issue:
Conduit kit for ATV12

Product Line:
ATV12, Altivar 12 Machine drive

Resolution:
The ATV12 drives do not have a NEMA 1 conduit kit option available.  The drive will need to be mounted inside a separate enclosure.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Attachment(s)
ATV12 Wiring.png [180.87 KB]