Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the part numbers for the replacement cooling fans for the ATV61 and ATV71 drives?
Issue:
ATV61 and ATV71 replacement part numbers for cooling fans

Product Line:
Altivar ATV61 and ATV71 open type drives

Environment:
All

Cause:
Needs a replacement cooling fan for the ATV61 and ATV71 drives.

Resolution:
See attachments

Schneider Electric Nigeria

Attachment(s)
Frame size 2 to 8 Fan Part numbers.png [327.74 KB]
Frame size 11 to 10 Fan Part numbers.png [234.56 KB]
Frame size 3 to 15 Fan Part numbers.png [263.25 KB]