Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is included in the ATVPOT25K potentiometer kit?
Issue:
ATVPOT25K potentiometer kit

Product Line:
Altivar accessory

Environment:
All models

Cause:
None

Resolution:
The ATVPOT25K pot kit is for use with any Altivar VFD.  It includes:
Potentiometer 22mm operator, ZB5AD922
Potentiometer, 80442-273-02, 2.5k Ohm
Legend holder, ZBZ32
Legend and Misc hardware not offered separately.

The pot operator has graduation marks only, no designations. The legend is marked "Manual-Speed Pot".

Schneider Electric Nigeria

Attachment(s)
ATVPOT25K.png [154.55 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings