Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we have any MTBF data on the ATV212 drives?
Issue:
MTBF data on the ATV212 drives

Product Line:
Altivar ATV212

Environment:
All

Cause:
Needs to know if we have any MTBF data on the ATV212 drives.

Resolution:
See the attached document.  Please note that this data does not include the heat sink cooling fan.

MTTF ATV212

This document gives the mean time to failure (MTTF) values of Altivar 212 variable speed drives.

Altivar 212 MTTF values are based on IEC 62380.
The fan is an aging part to replace in maintenance. Hence the fan is not taken into account in these MTTF values.
Voltage Kw MTTF values
Three 240V (M3X)0.75560000
1.5560000
2.2560000
3540000
3.7540000
5.5540000
7.5540000
11500000
15500000
18.5500000
22430000
30350000
Three 500V (N4)0.75560000
1.5560000
2.2560000
3540000
3.7540000
5.5540000
7.5540000
11540000
15500000
18.5500000
22400000
30400000


MTTF= MUT1= Mean Time To (first) Failure
MUT= Mean of MUTI= Mean Up Time
MDT= Mean of MDTI= Mean Down Time
MTBF= MUT+MDT= Mean Time between Failures

Schneider Electric Nigeria

Attachment(s)
MTBF ATV212.png [18.15 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings