Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What causes error "Unknown header in the file:" when downloading Unity firmware?
Issue:
Dowloading Unity copro or executive firmware displays error.

Resolution:
If flashing the CoPro firmware, make sure you are using FTP protocol.
If NOE, use FTP protocol.
Is the .bin / .ldx file correct for the PLC type?