Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you share symbols between a SoMachine Basic / Machine Expert Basic Project and a Vijeo-Designer Project ?
Before sharing the symbols with a Vijeo-Designer project, verify that all symbols that you want to share are defined in the SoMachine Basic / Machine Expert Basic project. If not, create/open a project in SoMachine Basic / Machine Expert Basic, define the symbol names, and save the product.
Follow these steps to share SoMachine Basic / Machine Expert Basic symbols with a Vijeo-Designer project:
Step
1
Start Vijeo-Designer.
2
Create/open a project in Vijeo-Designer.
3
Click the Project tab in the Navigator window, right-click IO Manager and select New Driver... Insert.
Result: The New Driver window opens.
4
Select a driver from the Driver list, select an equipment from the Equipment list, and click OK.
For example:
  • Driver: Modbus TCP/IP
  • Equipment: Modbus Equipment
Result: The Equipment Configuration window opens.
5
Enter the details for each parameter and click OK. For example, IP Address, Unit ID, IP Protocol, and so on. Make sure you check "IEC61131 Syntax" checkbox
Result: A new driver is created to open the communication with the controller. The selected driver and the selected equipment appear under the IO Manager node in the Project tab of the Navigator window.
6
In the Vijeo-Designer menu bar, click Variable → Link Variables.
Result: The Link Variable window opens.
7
Select the Files of type filter to SoMachine Basic / Machine Expert Basic project files (*.SMBP) and select the Equipment filter to the driver that you have created for communication.
8
Select the SoMachine Basic / Machine Expert Basic project in which you have defined the symbols and click Open.
Result: All the symbols are automatically extracted from the project and linked to the driver that you have created.
9
Select the variables that you want to use and add them to your HMI application.
Result: All the variables with same names as symbols are added in the list of available variables. The variable list appears under the Variables node in the Project tab of the Navigator window.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)