Issue:
Available communication options
Product Line:
ALTIVAR 61, ALTIVAR 71, ALTIVAR 312, ALTIVAR 32, ALTIVAR 212, ALTIVAR 12, ATV600, ATV320, ATV340, ATV900
Environment:
All drives all serial number
Cause:
N/A
Resolution :
The standard communication protocols are Modbus on all Schneider Drives. However, on the ALTIVAR 61, ALTIVAR 71, ALTIVAR 312, and ALTIVAR 32, ATV320, ATV340, ATV600, ATV900 CanOpen is also standard. the ATV600 has embedded Modbus Ethernet TCP/IP, The ATV340(E) version and the ATV900 have embedded Ethernet TCP/IP and Ethernet IP as standard.
Available communication options
Product Line:
ALTIVAR 61, ALTIVAR 71, ALTIVAR 312, ALTIVAR 32, ALTIVAR 212, ALTIVAR 12, ATV600, ATV320, ATV340, ATV900
Environment:
All drives all serial number
Cause:
N/A
Resolution :
The standard communication protocols are Modbus on all Schneider Drives. However, on the ALTIVAR 61, ALTIVAR 71, ALTIVAR 312, and ALTIVAR 32, ATV320, ATV340, ATV600, ATV900 CanOpen is also standard. the ATV600 has embedded Modbus Ethernet TCP/IP, The ATV340(E) version and the ATV900 have embedded Ethernet TCP/IP and Ethernet IP as standard.
Released for: Schneider Electric Nigeria