Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What would be a reason to adjust the analog input bias or analog input gain on an ATV212 Drive?
Issue:
Bias and gain adjustment on ATV212

Product Line:
ATV212

Environment:
All models and serial numbers

Cause:
None

Resolution:
One reason for changing the analog input bias and gain is that the speed reference signals may not be linear.
Example: If the drive is being sent a speed reference of 4mA signal with low speed (LL) at 0 hz but the drive runs above 0 hz. parameter F470 can be adjusted down so that the drive runs at 0 hz.  Or, on the upper end of the 4-20mA scale if the drive is being sent 20mA and the frequency only goes to 59 hz parameter F471 can be adjusted up to that the speed reaches 60 hz.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings