Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does ATS48 have Ethernet IP option?
Issue:
Do Schneider Electric drives connect to Allen Bradley Blue Hose protocol?

Product line:
Altistart ATS48, ATS22

Environment:
All models, all serial numbers

Cause:
Need to connect to Ethernet IP

Resolution:
Yes. EGX150 - Link150 Ethernet Gateway or contact 3rd party such as ProSoft or AnyBus for a Modbus to Ethernet IP Gateway.