How can we help you today?

How to migrate an installed library to other pc/unity?

Because some current version of library are not support to install in windows8.1 environment, so customer need a workaround to migrate the library from other pc's Unity to the Unity in a windows8.1 pc.
Please refer to the following steps:
1/ install the library by installation package in a PC with Unity pro software;
2/ open Unity pro ->tool->type library manager, find the installed library;
3/ right click the installed library -> create installable family -> to export the installed library as a installable family in a folder;
4/ copy the exported family files to another pc;
5/ using Unity tool "type library update" to install the library family in Unity.
For more detailed steps, please see the attached doc.

Schneider Electric Nigeria

Attachment(s)
Procedure to Migrate blocks to unity8.1..docx [400.66 KB]
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings