Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
The maximum values for Outlet Group Off delay and Minimum Return Runtime are inconsistent between the UPS LCD and PowerChute Agent

Issue:
In PowerChute Agent, Outlet Group Off delay and Minimum Return Runtime cannot be set to values greater than 9999, yet the same fields can be set to values greater than 9999 on the UPS LCD.

Product Line:
PowerChute Serial Shutdown v1.x
PowerChute Business Edition versions 9.0, 9.0.1, 9.1.0, 9.1.1, 9.2.0, 9.2.1, 9.5, 10.x

Environment:
OS: Linux, Solaris, Windows

Cause:
An upper limit of 9999 seconds (2 Hours, 46 minutes, and 39 seconds) has been set in PowerChute  Agent for the Outlet Group Off delay and Minimum Return Runtime. The UPS LCD supports an upper limit of 32767 for these fields.

Solution:
Use a value of 9999 or less when setting the Outlet Group Off delay and Minimum Return Runtime fields directly on the UPS LCD.