Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the F10 fault on a TR Inverter/Charger?

Environment:

12V or 24V DC battery systems

Cause:

F10 indicates a high battery voltage condition:

Above 15.5 V on a 12 V system
Above 31 V on a 24 V system

This typically occurs when the batteries are wired incorrectly, or an external charging source is pushing the voltage too high.

Resolution

Verify the batteries are connected in the correct configuration for the system (12V or 24V).
Check for external chargers, alternators, or solar controllers causing over‑voltage.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: