Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find information on the sw100, sw101, sw102 and sw103 dip switches on the ATV212 drives?
Issue:
ATV212 information from the SW101, SW102, and SW103 dip switches.

Product Line:
Altivar ATV212

Resolution:
There are 5 dip switches on the ATV212 drives
SW101= FM analog output U= voltage output I = current output
SW102= Sink Source switch
SW103= Term Switch. Selection of communication terminal resistor. When SW103 is set to Term, internal 120 Ohm termination resistor is connected between A and B terminals.
SW100= VIA= VIA analog input switch (U= voltage input or I= current input)
VIB= VIB analog input switch (0-10-vdc input or PTC input)

screenshot screenshot

screenshot screenshot

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings