Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find programming assistance setting up an Lonworks card on the S-Flex ATV212 drives?
Issue:
Looking for programming assistance, setting up a Lonworks card on the S-Flex ATV212 drives.

Product Line:
Altivar ATV212 or S-flex 212 drive

Environment:
All

Cause:
Needs to set up the Lonworks card on the ATV212 drive


Resolution:
Reference the ATV212 Lonworks programming manual ATV212_Lonworks_manual_EN_S1A53848_01

manual


Schneider Electric Nigeria

Attachment(s)
atv212_lonworks_manual_en_s1a53848_01.pdf [3.05 MB]