Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can the logic inputs status of the Altivar Drives be monitored via network communications?
Issue:
Wanting to know how can the logic inputs status of the Altivar Drives be monitored via network communications?

Product Line:
ATV61, ATV71, ATV32

Environment:
All Serial numbers

Cause:
N/A

Resolution:
The logic input status can be monitored by Modbus address 5202.
Bit 0 - LI1
Bit 1 - LI2
Bit 2 - LI3
Bit 3 - LI4
Bit 4 - LI5
Bit 5 - LI6
If extended IO cards are used
Bit 6 - LI7
Bit 7 - LI8
Bit 8 - LI9
Bit 9 - LI10
Bit 10 - LI 11
Bit 11 - LI 12
Bit 12 - LI 13
Bit 13 - LI 14