Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What IIS Components are required for SPM 7.0/PME 7.2 installation?
Issue
The customer wants to know what components are required to be installed prior to performing SPM/PME installation, and they also want to verify that all components were installed correctly during the process.

Product Line
Struxureware Power Monitoring 7.0
Power Monitoring Expert 7.2

Environment
Web Applications

Cause
Uninstalling, or missing components would cause some segments of the Web Application not to function properly.

Resolution

The following sections need to be installed prior to starting the SPM/PME installation:

i) Common HTTP Features
  • Static Content
  • Default Document
  • Directory Browsing
  • HTTP Errors
ii) Health and Diagnostics
  • HTTP Logging
  • Request Monitor
iii) Security
  • Request Filtering
iv) Performance Features
  • Static Content Compression
v) Management Tools
  • IIS Management Console

e) In addition, the followings are installed:
i) Application Development Features
  • (1) ASP.NET
  • .NET Extensibility
  • (3) ASP
  • (a) If prompted to add other role services, required by selections, click “Add Required Role Services”.
  • (4) ISAPI Extensions
  • (5) ISAPI Filters
  • ii) Management Tools
(1) IIS 6 Management Compatibility
  • IIS 6 Metabase and IIS configuration compatibility
  • IIS 6 WMI Compatibility
  • IIS 6 Scripting Tools

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings