Issue:
ENT button on ATV61/ATV71 when using the VW3A1101 HMI
Product Line:
Altivar ATV61 and ATV71 or any drive using the VW3A1101 for programming.
Environment:
All
Cause:
Need to know how to save the parameters after entering data into the drive.
Resolution:
The enter or ENT button is the large round knob on the W3A1101 keypad. Just push the wheel to enter.
ENT button on ATV61/ATV71 when using the VW3A1101 HMI
Product Line:
Altivar ATV61 and ATV71 or any drive using the VW3A1101 for programming.
Environment:
All
Cause:
Need to know how to save the parameters after entering data into the drive.
Resolution:
The enter or ENT button is the large round knob on the W3A1101 keypad. Just push the wheel to enter.
Released for: Schneider Electric Nigeria