Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Should the drive or softstarter be disconnected prior to meggering the motor or motor wires?
Issue:
Drive or softstarter recommendation prior to meggering the motor or motor wires

Product Line:
All variable frequency drives and soft starts

Environment:
All models and serial numbers

Cause:
Meggering the motor

Resolution:
Yes, the drive or soft start must be disconnected before a megger test is performed on the motor or motor wires.