Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you use the ATV12 drive on 230vac single phase input and get 230vac 3 phase output?

Article available in these languages: Spanish

Issue:
Using an ATV12 drive on 230vac 1 phase input and getting 230vac 3 phase output.

Product Line:
Altivar 12

Environment:
All

Cause:
Needs to feed the drive 1 phase input and have 3 phase voltage coming out of the drive.

Resolution:
The ATV12 version with suffix M2 is designed for 230vac single phase input and will produce a 230vac 3 phase output.
The ATV12 version with suffix M3 is not designed or rated for single phase supply.

Note that all Altivar drives are designed to control / run 3phase motors.  They are not designed for phase converter applications to power a machine that includes various loads such as contactors, transformers, relays, heaters, pilot lights etc...