Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Procedure on How to Use OPC Test Client

Issue
An OPC Client does not read values from the OPC Server provided by Power Monitoring Expert (PME).  As such it is necessary to verify OPC Server is functioning properly.  For this purpose, OPC Test Client, a utility provided by PME can be used.

Product Line
Power Monitoring Expert (PME)

Environment
OPC

Cause
Testing OPC Server capability of PME to verify its functionality.

Resolution
1. Run OpcTestClient.exe from ...\system\bin\ in PME installation folder.

2. Click on 'Connect' button on the right side.

Note that the OPC Server address (opcda://localhost/ION.OpcDaServer) is already selected in the 'Server' drop down list.  If not, it should be selected from the drop down list:

server in opc test client

Upon connection, ION.OpcDaServer will appear in the left pane:

the server name

3. Right click on ION.OpcDaServer and select 'Create Subscription...':

create subscription

4. Provide a name for the subscription and click Next:

provide name here

The devices will populate on the left side:

where devices populate

5. Select a measurement from a device.  Double click on the tag to transfer it to the right pane:

device tag

6. Click Next:

what to click to proceed

7. Click Done to see the value:

the value is displayed

Note* There is no link to OPC Test Client. It can be found in the installation folder created by the PME software.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings