Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unity help incorrectly states that the outputs on the BMXDDI1602 are isolated.
Issue
Unity help incorrectly states that the outputs on the BMXDDI1602 are isolated.

Product Line
x80 Modules, EcoStruxure Control Expert (formerly known as Unity Pro)

Environment
Windows 7 Professional, Unity Pro 8.1, BMXDDI1602.

Resolution
  • Unity help incorrectly shows that the outputs on the BMXDDI1602 are isolated.



  • The wiring diagram from the user manual correctly shows the outputs as not being isolated.


Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings