Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use a different line voltage than what my drive is rated for?
Issue:
Different line voltage usage for Altivar Drives.

Product Line:
Altivar drives

Environment:
All models

Cause:
None

Resolution:
Drives that are rated for a specific line voltage range should only be operated within that range. Attempting to operate a drive outside this range will result in an under supply fault or over supply fault.
Line voltage tolerance is +10% and -15%.

For example: With a 460V drive the line voltage tolerance range would be 391VAC to 506VAC.