How to resolve the "ETY410" issue during CRA312/CRP312 firmware upgrading.
Summary:
Many engineers are likely to come across the "ETY410" issue during CRA312/CRP312 firmware upgrading. Namely, they could not continue the upgrading procedure due to the hardware id mismatch
by showing "ETY410"
Solution:
Actually, there are two issues mixed:
1. 140CRA31200, we have to use unity loader instead of OS loader to carry out the firmware upgrade. By OS loader , since /FLASH0/fw/fw.ini is not available, it display
the default info ETY410
2. 140CRP31200, it is ok to carry out the firmware upgrading by the OS loader. However, the firewall/anti-virus software might impede the proper message enquiry via
OS loader to module, there is chance that the identification failed & default name ETY410 was shown. Shut down the firewall/anti-virus & try again would solve the problem.
Many engineers are likely to come across the "ETY410" issue during CRA312/CRP312 firmware upgrading. Namely, they could not continue the upgrading procedure due to the hardware id mismatch
by showing "ETY410"
Solution:
Actually, there are two issues mixed:
1. 140CRA31200, we have to use unity loader instead of OS loader to carry out the firmware upgrade. By OS loader , since /FLASH0/fw/fw.ini is not available, it display
the default info ETY410
2. 140CRP31200, it is ok to carry out the firmware upgrading by the OS loader. However, the firewall/anti-virus software might impede the proper message enquiry via
OS loader to module, there is chance that the identification failed & default name ETY410 was shown. Shut down the firewall/anti-virus & try again would solve the problem.
Released for: Schneider Electric Nigeria




Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.