Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to compare two programs / projects in SoMachine versions 4.1, 4.2 or 4.3?
In SoMachine versions 4.1, 4.2 or 4.3 you can use the command located under the Logic Builder / Project / Compare to compare the actual project with another one (reference project). The reference project and the compare options are specified in the Project Compare dialog box, which opens, when the command is executed.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings