Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
After an upgrade from PME 7.2.x to PME 8.0 I can no longer see background images in WebReach
Issue:
Customer has performed a side-by-side or in-place upgrade from PME 7.2.x. They are able to see all their backgrounds in vista, but when they navigate to WebReach, all the images in the JPEG format don't appear. The images in the BMP format appear correctly. They are specifying the image location via an UNC path as they configure screens using engineering clients.

Product Line:
Power Monitoring Expert 8.0

Environment:
Power Monitoring Expert Software Upgrade
Vista Screen Configuration
WebReach
Engineering Client

Cause:
This is a known issue with PME8 that was caused by adding support for PNG and GIF background images in Vista.

Resolution:

*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).


Close all instances of WebReach, and rename the WebReach.dll file located in the ...\Power Monitoring Expert\system\bin folder. Place the attached file in the same folder. Restart WebReach to see the changes.

Schneider Electric Nigeria

Attachment(s)
WebReach.dll [81.5 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings