Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an operation in Unity Pro that replaces the Concept M1HEALTH function block?

No.
The Concept M1Health function block was used to monitor local IO and distributed IO Bus servers.
All of the same functionality can be reproduced in Unity Momentum with System Words.
Local IO Base can be monitored using %S119.
IO Bus Health can be monitored using %S118.
Server Module Health can be monitored using %SW128, %SW129.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)